2017-08-04 1:22 AM
I want to use FOC LIB to develop my application, but I found FOC LIB used Std Drvier, STM32CubeMX used HAL Drvier. Does STM32 HAL Drvier support STM32 PMSM FOC LIB ?
#foc-sdk-4.3.0 #hal-driver2018-01-03 5:29 AM
I was about to use a DMA example from STM32Cube_FW_F3_V1.8.0 in my FOC application based on STM32 PMSM FOC LIB_4.3 when I realized what Jarvis Xing describes: FOC lib is using std drivers - not HAL..
In general, I would like to use several examples from the STM32Cube_FW into my FOC-application.
So basically, I have the same question as Jarvis Xing, but I would like to check if somebody has some advices or comments to following alternatives:
2018-01-03 7:04 AM
Hi
Holm.Gunnar
, is developed based on HAL drivers. Why don't you use it?Are some algorithms that you need missing there?
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2018-01-03 3:06 PM
As I understand, the x-cube-spn7 uses six step control only - and (UM1945) refers to the ST FOC SDK for FOC control (which is what I want to run). Also, I find the MC workbench SW very useful.
In fact, alternative 3 seems ok - the std drivers includes a 'how to use' description and the basic dma function is now up and running.