2017-08-28 1:35 PM
I generated a new project selecting Nucleo H743 , set the RCC to 8Mhz and made sure that USB is clocked at 48Mhz just like I did on the F767. Unfortunately the device does not show up in the windows device manager.
Does somebody have a working USB device example of any kind on the Nucleo H743 ?
Any ideas ?
I have attached the CubeMX project file.
Thanks for your help !
#usb-fs #stm32h7Solved! Go to Solution.
2017-08-29 11:56 AM
I found the problem. The peripheral clocks need to be initialized each separately because
in stm32h7xx_hal_rcc_ex.c it is selected with
if((PeriphClkInit->PeriphClockSelection) == RCC_PERIPHCLK_USB)
for the F7 it used to have the format
if(((PeriphClkInit->PeriphClockSelection) & RCC_PERIPHCLK_USB) == (RCC_PERIPHCLK_USB))
2017-08-29 11:56 AM
I found the problem. The peripheral clocks need to be initialized each separately because
in stm32h7xx_hal_rcc_ex.c it is selected with
if((PeriphClkInit->PeriphClockSelection) == RCC_PERIPHCLK_USB)
for the F7 it used to have the format
if(((PeriphClkInit->PeriphClockSelection) & RCC_PERIPHCLK_USB) == (RCC_PERIPHCLK_USB))
2017-09-13 8:57 AM
Hi
Amann.Joerg
,You are right. There is an issue in
http://www.st.com/en/embedded-software/stm32cubeh7.html
V1.0.0 with the function HAL_RCC_ClockConfig().To make it work as it is implemented, you need to modify the code generated with
http://www.st.com/en/development-tools/stm32cubemx.html
:unroll and loop on each RCC_ClkInitStruct.ClockType definition within SystemClock_Config() before calling HAL_RCC_ClockConfig() (i.e. call HAL_RCC_ClockConfig() with only one ClockType defined, not using OR operator).
This will be corrected with the upcoming STM32CubeH7 V1.1.0 to be published on st.com.
Best regards,
Cedric