2025-09-02 4:49 PM
Hello,
I saw a thread titled
And I tried to enter to the examples selector of CubeIde (I never tried before).
When I open the selector, my computer takes several minutes with the cpu fan at highest speed.
After this, I tried to select a board to reduce posibilities, and happened the same, but I had a memory full error.
The only way to continue is to kill CubeIde. It's impossible to close it safely.
But now CubeIde does not start. It ask me the workspace, and shows the picture of screenshot I attached.
If I select a different workspace, it works.
And now, my questions are...
Can I restore my workspace? Seems all project files are present.
Do I need more memory?
My system is:
Linux mint 21.3, Linux 5.15.0-153
Intel i7-8700K @3.7GHz (6 core, 12 threads)
16GB RAM
CubeIde 1.15.0
Thanks for your reply
2025-09-02 6:25 PM
1.15.0 is pretty old.
ST currently has v1.19.0
Try un-installing the old version and install the new version. You should be able to select your workspace.