2016-12-06 6:04 AM
Hi,
I was checking through the implementation of osSignal in the file installed by STM32CubeMX to 'Middlewares/Third_Party/FreeRTOS/Source/CMSIS_RTOS/cmsis_os.c'
The
http://www.keil.com/pack/doc/CMSIS/RTOS/html/group__CMSIS__RTOS__SignalMgmt.html
specifies that the call to osSignalWait will 'Suspend the execution of the current
runningthread until ALL specified signal flags with the parametersignalsare set.'This is exactly the behavior of the FreeRTOS function
http://www.freertos.org/xEventGroupWaitBits.html
. However, in the osSignal implementation, the FreeRTOS primitive 'TaskNotify' is used. As noted onhttp://www.freertos.org/RTOS_Task_Notification_As_Event_Group.html
, 'Unlike when using an event group the receiving task cannot specify that it only wants to leave the Blocked state when a combination of bits are active at the same time. Instead the task is unblocked when any bit becomes active, and must test for bit combinations itself.'This means that the osSignal functionality does not behave as specified.
Please let me know if I have misunderstood the situation, or please let me know how this can be fixed?
Cheers,
Oskar
#cmsis-rtos #freertos2017-04-05 4:15 AM
,
,
My understanding is that if you want to write code which is compatible with
both official cmsis documentation and STM32 implementation, you must use
this API 1 bit at a time when waiting and reading, and not use
osSignalClear (which is not implemented, and I suspect it would not be safe
anyway).
Since osSignalClear
<,http://www.disca.upv.es/aperles/arm_cortex_m3/curset/CMSIS/Documentation/RTOS/html/group___c_m_s_i_s___r_t_o_s___signal_mgmt.html ♯ gafcb3a9bd9a3c4c99f2f86d5d33faffd8>,
unimplemented,
the only chance to clear a signal is through osSignalWait
<,http://www.disca.upv.es/aperles/arm_cortex_m3/curset/CMSIS/Documentation/RTOS/html/group___c_m_s_i_s___r_t_o_s___signal_mgmt.html ♯ ga38860acda96df47da6923348d96fc4c9>,
.
So, if you wait
In your example, you must repeat the wait for MY_EXTRA_FLAG, or it will
never be reset.
2017-04-05 10:44 GMT+02:00 Richard Lowe <,st-microelectronics@jiveon.com>,:
STMicroelectronics Community
<,https://community.st.com/?et=watches.email.thread>,
Re: CMSIS RTOS feature osSignal incorrectly implemented on FreeRTOS
reply from Richard Lowe
<,https://community.st.com/people/Lowe.Richard?et=watches.email.thread>, in *STM32
MCUs Forum* - View the full discussion
<,https://community.st.com/message/153480-re-cmsis-rtos-feature-ossignal-incorrectly-implemented-on-freertos?commentID=153480&,et=watches.email.thread ♯ comment-153480>,
2017-04-05 6:13 AM
Well yes and no on the wait. For this example, I have a periodic task that happens after so much time has expired, but not time critical. So the timer expires and sets off the flag. Then when it gets around to it, the 'more magic' happens.
You could do it this way:
osEvent evt;
for(;;)
{
evt = osSignalWait( 0x00, osWaitForever );
if( evt.value.signals & MY_GO_FLAG)
{
...magic goes here.
}
else if( evt.value.signals & MY_EXTRA_FLAG )
{
... more magic happens.
}
}�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
That would wait for ANY flag and then you would check for that particular flag during execution.
2017-04-05 2:19 PM
In my understanding, osSignalWait (0x00, osWaitForever) will not reset the
flags. But I did not test.
2017-04-05 14:24 GMT+02:00 Richard Lowe <st-microelectronics@jiveon.com>:
STMicroelectronics Community
<https://community.st.com/?et=watches.email.thread>
Re: CMSIS RTOS feature osSignal incorrectly implemented on FreeRTOS
reply from Richard Lowe
<
MCUs Forum* - View the full discussion
<https://community.st.com/0D70X000006Sy3KSAS
2017-04-05 3:04 PM
Seems to clear in my application but...
pxCurrentTCB->ulNotifiedValue &= ~ulBitsToClearOnExit;�?�?
From the call to FreeRTOS:
xTaskNotifyWait
But you might be correct. A flag check of 0x00 might not clear the flag.
2017-04-05 5:03 PM
What is the value of ulBitsToClearOnExit ?
Il Mer 5 Apr 2017, 22:05 Richard Lowe <st-microelectronics@jiveon.com> ha
scritto:
STMicroelectronics Community
<https://community.st.com/?et=watches.email.thread>
Re: CMSIS RTOS feature osSignal incorrectly implemented on FreeRTOS
reply from Richard Lowe
<
MCUs Forum* - View the full discussion
<https://community.st.com/0D70X000006T0IwSAK
2019-01-16 10:01 PM
Posting to update the status of this issue.
ST's implementation still doesn't allow waiting for more than one signals at a time and will return with osEventSignal when even one is sent.
2020-03-17 8:01 AM
Old thread, but I thought I would post this here in case this hasn't been fixed.
I ran into this problem and made the following change to the Freertos call to xTaskNotifyWait in wrapper file cmsis_os.c
The change to the first parameter clears any bits in the calling threads notification value on entry. The original call is commented out.
In the original call no bits are cleared ( param 1 = 0 ) and as is mentioned above, the osSignalClear() function is not implemented.
osEvent osSignalWait (int32_t signals, uint32_t millisec)
{
osEvent ret;
#if( configUSE_TASK_NOTIFICATIONS == 1 )
TickType_t ticks;
ret.value.signals = 0;
ticks = 0;
if (millisec == osWaitForever) {
ticks = portMAX_DELAY;
}
else if (millisec != 0) {
ticks = millisec / portTICK_PERIOD_MS;
if (ticks == 0) {
ticks = 1;
}
}
if (inHandlerMode())
{
ret.status = osErrorISR; /*Not allowed in ISR*/
}
else
{
//if(xTaskNotifyWait( 0,(uint32_t) signals, (uint32_t *)&ret.value.signals, ticks) != pdTRUE)
if(xTaskNotifyWait( 0xFFFFFFFF,(uint32_t) signals, (uint32_t *)&ret.value.signals, ticks) != pdTRUE)
{
if(ticks == 0) ret.status = osOK;
else ret.status = osEventTimeout;
}
else if(ret.value.signals < 0)
{
ret.status = osErrorValue;
}
else ret.status = osEventSignal;
}
#else
(void) signals;
(void) millisec;
ret.status = osErrorOS; /* Task Notification not supported */
#endif
return ret;
}
2021-11-27 8:20 AM
Discovering this thread 2 years later: so to clarify, does the above change remove the need for an osSignalClear() function/call? (does clearing all bits effectively clear the signal?)