2020-07-18 2:36 AM
I am using LWIP 2.1.2 in stm32f769I discovery board.
I can ping IPv4 from my PC.
But i can't ping IPv6.
I have enabled the Autoconfig(Stateless).
As per my understanding the IP address will be created based on the MAC.
My MAC is 00:80:e1:00:00:00
Link local address is fe80::280:e1ff:fe00:0000
I tried to ping this address from my PC.
But host is unreachable.
IPv4 is working but IPv6 is not working.
I have attached my code below.
Please tell me how to solve this issue.
Thanks in advance.
///////////////////////////////////////////////////////////////////////////////////////////////
void MX_LWIP_Init(void)
{
/* IP addresses initialization */
IP_ADDRESS[0] = 192;
IP_ADDRESS[1] = 168;
IP_ADDRESS[2] = 0;
IP_ADDRESS[3] = 102;
NETMASK_ADDRESS[0] = 255;
NETMASK_ADDRESS[1] = 255;
NETMASK_ADDRESS[2] = 255;
NETMASK_ADDRESS[3] = 0;
GATEWAY_ADDRESS[0] = 0;
GATEWAY_ADDRESS[1] = 0;
GATEWAY_ADDRESS[2] = 0;
GATEWAY_ADDRESS[3] = 0;
/* Initilialize the LwIP stack with RTOS */
tcpip_init( NULL, NULL );
/* IP addresses initialization without DHCP (IPv4) */
IP4_ADDR(&ipaddr, IP_ADDRESS[0], IP_ADDRESS[1], IP_ADDRESS[2], IP_ADDRESS[3]);
IP4_ADDR(&netmask, NETMASK_ADDRESS[0], NETMASK_ADDRESS[1] , NETMASK_ADDRESS[2], NETMASK_ADDRESS[3]);
IP4_ADDR(&gw, GATEWAY_ADDRESS[0], GATEWAY_ADDRESS[1], GATEWAY_ADDRESS[2], GATEWAY_ADDRESS[3]);
/* add the network interface (IPv4/IPv6) with RTOS */
netif_add(&gnetif, &ipaddr, &netmask, &gw, NULL, ðernetif_init, &tcpip_input);
/* Create IPv6 local address */
netif_create_ip6_linklocal_address(&gnetif, 1);
netif_ip6_addr_set_state(&gnetif, 0, IP6_ADDR_VALID);
gnetif.ip6_autoconfig_enabled = 1;
netif_set_default(&gnetif);
if (netif_is_link_up(&gnetif))
{
/* When the netif is fully configured this function must be called */
netif_set_up(&gnetif);
}
else
{
/* When the netif link is down this function must be called */
netif_set_down(&gnetif);
}
///////////////////////////////////////////////////////////////////////////////////////////////
2025-03-05 5:28 AM
Were you able to fix it? The same thing happens to me.