2010-01-06 3:10 AM
2011-05-17 4:30 AM
Hi Niko,
I reported the previous bug to Microsupport, and they are informing the maintainers. I will look into this one also and try and report on the same ticket. Martin.2011-05-17 4:30 AM
I don't know much about USB, but I thought there would have been more help available for this chip. Even with the onboard peripheral, there sure is a lot of extra code required! It doesn't help that the STM32_OTG_LIB.pdf file is very very sparse on details for beginners! And why is their demo project in binary form?
I'm trying to do a basic FAT file system on a USB memory stick. I thought this would be a basic project, but I'm getting lost in Atmel's USB code. I'm using Chan's FAT (http://elm-chan.org/fsw/ff/00index_e.html), so I just need to implement a few functions:2011-05-17 4:30 AM
Hi All,
These 2 bugs have been reported the MCU support europe. I am told this will be fixed in the next release. Cheers, Martin.2011-05-17 4:30 AM
Hi Sheldon,
I believe the stack itself is 3rd party, which could explain absence of source code (except for the driver). From memory it may be Micrium's, but it does not mention that in the docs. Atmel's USB code? (Do you mean ST maybe :) ) Which compiler are you using? Cheers, Martin.2011-05-17 4:30 AM
2011-05-17 4:30 AM
Hi Martin,
Yeah - I meant ST. I just finished another project with an Atmel uP :) I'm using IAR for this project. I just had an Arrow Sales Rep give me the rundown on the Stellaris family of processors - and after going through their demo with a USB flash drive and full source code, I'm starting to wonder if I should switch. So is it going to be that much work to get USB MSD with a FAT driver on this processor without using an RTOS?2011-05-17 4:30 AM
Hi Sheldon,
I don't know how difficult this would be to write, but my instinct tells me a USB analyzer would be usefull :). I am trying to obtain a bit more information about this, and will post when I have found out more. Martin.2011-05-17 4:30 AM
Hi,
I have problem in porting usb driver to STM32F105RCT. The situation details wrote to google doc of Following URL, and send question to st-micro technical support now. http://docs.google.com/View?id=dfnf3mhx_41nk8bwdf92011-05-17 4:30 AM
Do you know the schedule for the release of new USB libs?
2011-05-17 4:30 AM
Dear all,
We are planning to fix this corner case in our next release on STM32105/7 devices USB peripheral device examples, and it would be scheduled for April 2010. Cheers, STOne-32.