BUG in stm32f4xx_hal_rcc_ex.h
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2019-08-21 5:53 AM
In function
uint32_t HAL_RCCEx_GetPeriphCLKFreq(uint32_t PeriphClk)
string
/* Get the current I2S source */
srcclk = __HAL_RCC_GET_I2S_SOURCE();
must be
/* Get the current I2S source */
srcclk = __HAL_RCC_GET_I2S_SOURCE() ? RCC_I2SCLKSOURCE_EXT : RCC_I2SCLKSOURCE_PLLI2S;
because __HAL_RCC_GET_I2S_SOURCE() return RCC_CFGR_I2SSRC_Msk if bit RCC_CFGR_I2SSRC is set. But need RCC_I2SCLKSOURCE_EXT or RCC_I2SCLKSOURCE_PLLI2S in next
switch (srcclk)
{
/* Check if I2S clock selection is External clock mapped on the I2S_CKIN pin used as I2S clock */
case RCC_I2SCLKSOURCE_EXT:
...
case RCC_I2SCLKSOURCE_PLLI2S:
...
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-11-24 7:15 AM
Hello @NZhar,
A similar question is already asked here.
Internal ticket number: 139649 (This is an internal tracking number and is not accessible or usable by customers).
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.