BSP_AUDIO_OUT_Play ends up in Default_Handler
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-05-12 9:25 AM
Hello,
I try to play a sound using stm32h747i_discovery_audio.c. Initialization goes well
void CAudioController::AudioOutInit()
{
BSP_AUDIO_Init_t audioOutInit;
if (!audioOutInitDone_)
{
audioOutInit.Device = AUDIO_OUT_DEVICE_HEADPHONE;
audioOutInit.ChannelsNbr = 2;
audioOutInit.SampleRate = AUDIO_FREQUENCY_44K;
audioOutInit.BitsPerSample = AUDIO_RESOLUTION_16B;
audioOutInit.Volume = 50;
if (BSP_AUDIO_OUT_Init(0, &audioOutInit)!=BSP_ERROR_NONE)
{
while(1);
}
audioOutInitDone_ = true;
}
}
But first call BSP_AUDIO_OUT_Play call
BSP_AUDIO_OUT_Play(0,playBuf,1024);
ends up in the default handler. It is a bit strange but while debugging the program jumps to the default handler either from
HAL_DMA_Start_IT
call or from
__HAL_SAI_ENABLE_IT(hsai, SAI_InterruptFlag(hsai, SAI_MODE_DMA));
inside BSP_AUDIO_OUT_Play().
The BSP_AUDIO_OUT_Init() initializes Sai and DMA.
Does anybody have a hint in which direction to look for the root cause?
Best Regards,
Anton
Solved! Go to Solution.
- Labels:
-
Audio
-
STM32H7 Series
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-05-12 6:33 PM
Read the VECTACTIVE bits to determine which IRQ it wants to be in. Subtract 16 from that value to find the IRQn_Type. Chances are that IRQ is not implemented and is defaulting to Default_Handler.
IRQn_Type irq_handler = (IRQn_Type) ((SCB->ICSR & SCB_ICSR_VECTACTIVE_Msk) - 16);
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-05-12 6:33 PM
Read the VECTACTIVE bits to determine which IRQ it wants to be in. Subtract 16 from that value to find the IRQn_Type. Chances are that IRQ is not implemented and is defaulting to Default_Handler.
IRQn_Type irq_handler = (IRQn_Type) ((SCB->ICSR & SCB_ICSR_VECTACTIVE_Msk) - 16);
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-05-13 5:09 AM
Thanks for the hint! I saw that it was DMA2_Stream1 interrupt. I didn't really know what to do with it and just forwarded to the bsp audio handler. Surprisingly it worked. If any other stm newbie has the same problem here is the solution:
void DMA2_Stream1_IRQHandler(void)
{
BSP_AUDIO_OUT_IRQHandler(0);
}