2010-02-12 8:23 AM
2011-05-17 4:40 AM
Check the MAP/HEX files to confirm the base address of the application code.
It is important that the low order address bit of any code you jump to is 1, the STM32 can only execute THUMB code. I export the address of the vectors in the application start up code, then use that to set the address. So provided you don't violate any alignment rules, the application is agnostic to the location it is loaded. In the startup.s file EXPORT __Vectors In the application.c file extern void * __Vectors; NVIC_SetVectorTable((u32)(&__Vectors), 0x0); // Smart Base Location Some assembler to enter the system boot loader looks like this, change the address to reflect the base address of you application. Reboot_Loader PROC EXPORT Reboot_Loader LDR R0, =0x1FFFF000 LDR SP,[R0, #0] LDR R0,[R0, #4] BX R0 ENDP -Clive2011-05-17 4:40 AM
Could the odd boundary be my problem. I am locating code at 0x8004000 and attempting to run it.(on Even boundary). Don't know anything about thumb alignment. It is the entire binary that I am copying to this location.
My Code code was: void app_start(void) { void (*app)(); irq_disable(); runapp=(void(*)())(0x8004000); app(); } Replaced with the code you gave and still the same. I think IRQs are a distraction, it should still start? .arm .text global start_application start_application: ldr R0, =0x1FFFF000 ldr SP,[R0, #0] ldr R0,[R0, #4] BX R0 Thanks2011-05-17 4:40 AM
The code assumes you have the Stack Pointer and Start Address as the first two words of the image.
If the first half-word is an instruction, you would need to jump to 0x8004001, as you are running Thumb code, not ARM code. -Clive2011-05-17 4:40 AM
Sorry that address was
start_app: ldr R0, =0x8004000 ldr SP,[R0, #0] ldr R0,[R0, #4] BX R02011-05-17 4:40 AM
No Luck. The start of Rom where it is jumping to starts with the IRQ table
so I presume that can start at location:0x8004000 I have no memory protection stuff turned on. Does anyone know of any sample code that jumps to another location in Rom? (written in C):__attribute__ ((section(''.isr_vector''))) void (* const g_pfnVectors[])(void) = { (void (*)(void))((unsigned long)stack + sizeof(stack)), // The initial stack pointer ResetISR, // The reset handler NmiSR, // The NMI handler FaultISR, // The hard fault handler etc.2011-05-17 4:40 AM
You're going to need to examine the code/data generated by the compiler/linker. Unless the correct addresses and linkage is occurring this isn't going to work.
Try using aJTAG
debugger and single stepping the critical code to ensure it is doing what you expect. -Clive2011-05-17 4:40 AM
I have looked at AN2557 and there doesn't appear to be much in it.
I am using GCC, so the function NVIC_SetVectorTable(NVIC_VectTab_FLASH, 0x4000); doesn't appear to be available to me. Looking at the map file though, the vectors are located at 0x8004000 The definition is as follows: __attribute__ ((section(''.isr_vector''))) void (* const gpVectors[])(void) = { (void (*)(void))((unsigned long)stack + sizeof(stack)), and mapfile gives : .isr_vector 0x08004000 0x130 bin/startup.o 0x08004000 gpVectors So happy there. I thought that maybe it was an alignment issue. I copy the binary to 0x8004000 but maybe I should be runninfg the application from 0x8004001 (Bt the way, application runs fine without bootloader) My code to run application is: #define APP_ORIGIN 0x8004000 void app_start(void) { void (*runapp)(); irq_disable(); runapp=(void(*)())APP_ORIGIN; runapp(); } have also tried runapp=(void(*)())(APP_ORIGIN+1);2011-05-17 4:40 AM
I will study the sample app, this is useful.
I notice they run app_address+4 when running the application, tried it quickly, bur I still crash. I will left you know if I get success from the app note. Thanks2011-05-17 4:40 AM
Ok, you don't need to change the load location to 0x8004001, the low order bit simply flags to the program counter that the code in question is THUMB code. All code on the STM32 (Cortex-M3) must be THUMB, it cannot execute 32-bit ARM code.
Also remember that the first vector entry is the address of the stack top in RAM, the second entry is the reset vector. It is the address of the reset vector, not executable code. The assembler code to execute from a vector table would be LDR R0, =0x08004000 LDR SP,[R0, #0] LDR R0,[R0, #4] BX R0 If NVIC_SetVectorTable() is not available you will need to reprogram the NVIC directly to point the hardware to the vector table. -Clive