2025-03-27 2:23 AM
Hello everyone,
I use the NUCLEO-H743ZI2 board in my project and previously, Before I've used the MBed OS - it works well on this board, just I need to maximize TCP transfer speed as well as QSPI. So I decided to try another RTOS. After reading forums, I decided to try the Azure RTOS and Cube IDE. I chose the Nx_TCP_Echo_Echo_Server example as a starting point. I reconfigured it to use with NUCLEO-H743ZI2, and also I disabled DHCP as I don't need it. Also added plenty of printf functions at different steps in the app_netxduo.c. As result project can be build, and I see next messages in Terminal:
The network cable is connected.
nx_ip_interface_status_check == NX_SUCCESS.
nx_ip_address_set == NX_SUCCESS.
nx_tcp_socket_create == NX_SUCCESS .
nx_tcp_server_socket_listen == NX_SUCCESS .
TCP Server listening on PORT 5000
STM32 NX_APP_DEFAULT_IP_ADDRESS: 192.168.0.200
Next is the tx_semaphore_get
Then I try to ping the board I see the blinking LED on the Ethernet connector of the board but I get :
Ping statistics for 192.168.0.200:
Packets: Sent = 4, Received = 0, Lost = 4 (100% loss),
Thus, it looks like the function
static VOID tcp_listen_callback(NX_TCP_SOCKET *socket_ptr, UINT port)
{
tx_semaphore_put(&TCPSemaphore);
}never called.
I already spent two days trying to find solutions. All receipts which I found - like
https://community.st.com/t5/stm32-mcus/ethernet-not-working-on-stm32h7x3/ta-p/49479
I implemented them - the result is the same.
Does anyone have any idea where is the problem?
Thanks in advance.
2025-04-01 2:09 AM
@matt-crc
Thank you for your recommendations - but if you briefly read my posts in this thread, you will find that I already tried many things. When I decided to change MBed Os to another RTOS, I have spent some time and read plenty of forums - so the choice of Azure RTOS was made after thought. But after 10 days of trying, I still haven't made any progress with quite simple task - make a TCP server. So I'd like to stay on Azure, but I don't know how I'm going to get a working configuration for my board yet.
2025-04-04 11:17 PM
Wold help if I can provide a reference design from where you can start?
2025-04-06 11:40 PM
@mbarg.1 wrote:Wold help if I can provide a reference design from where you can start?
It will be very useful! I have ordered Nucleo-H723 for testing, but the H743ZI2 boards are already in the devices, so it will be good to use them.
Thank you in advance!
2025-04-07 1:45 AM
By the way, I succeed to start on H743ZI2 board the STM32_Nucleo_H723ZG_FreeRTOS_TCP example.
I can ping my board and get response from TCP server.
But still, Azure RTOS seems more attractive...
2025-04-07 1:46 AM
OK.
PLEASE:
Now you can have a look at the code - there are many lines which are part of our modular environment and you can remove them easily.
2025-04-07 7:05 AM
Thank you, Mike!
I successfully imported your project, compiled it - it was some minor problems, but finally as you wrote it was only one warning. I build project and run in debug mode. As result, I got response in the Putty, I also see some activity of the board in Wireshark, I found the IP address as you pointed out - and result, board do not respond to this IP. :( Disappointing.
See attached screenshots.
So I am going to return to Azure RTOS when I got NUCLEO-H723ZG board. For now, I lost enough time.
Once again for your help!
With best regards, Irek
2025-04-07 7:35 AM
Irek:
It looks like your STM32CubeIde installation is corrupted - indexer errors usually come from this - or did you use a non empty workspace or you do not have corect permission or an antivirus is blocking something...
By sure, NetXDuoEthIpInstance values does not make any sense, i do not believe you are on an non-local network.
Check what is going on in your environment or you will have same problems with H723.