2023-06-21 8:39 PM
I was under the impression the adc handler would by default generate a flag to exit the sleep mode. The interrupt never flags the exit. I know there is a parameter inside HAL_EnterSleepMode that will exit if there is a interrupt but it doesnt seem to trigger. Can someone provide insight or a simple example of how I would flag the exit of sleep mode properly w/o timer. (Using stm32u5 585 discovery board)