ADC Calibration Return Fails due to ADC_CALIBRATION_TIMEOUT on STM32G030X6
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-11-29 12:24 AM
First of all , I read this post (https://community.st.com/t5/stm32-mcus-products/adc-calibration-doesn-t-complete-on-stm32g0c1re/td-p/590459) that was previously opened on this subject. I think the issue is noy completly resolved because there is a misunderstanding.
I'm using STM32Cube MCU Package for STM32G0 Series, software package.
As @Imen.D replied on 2024-03-26 , 04:44 pm in this post (https://community.st.com/t5/stm32-mcus-products/adc-calibration-doesn-t-complete-on-stm32g0c1re/td-p/590459:(
- In fact, the delay is required for ADC disable to be effective (therefore, applicable between ADC disable and calibration start, or between ADC disable and calibration factor set).
I couldnt see delay placed in the relevant code sections.
Even if I put uS delays to those sections. It didnt work.
Here is the problem :
HAL_StatusTypeDef HAL_ADCEx_Calibration_Start(ADC_HandleTypeDef *hadc)
{
HAL_StatusTypeDef tmp_hal_status;
__IO uint32_t wait_loop_index = 0UL;
uint32_t backup_setting_cfgr1;
uint32_t calibration_index;
uint32_t calibration_factor_accumulated = 0;
uint32_t tickstart;
uint32_t adc_clk_async_presc;
__IO uint32_t delay_cpu_cycles;
/* Check the parameters */
assert_param(IS_ADC_ALL_INSTANCE(hadc->Instance));
__HAL_LOCK(hadc);
/* Calibration prerequisite: ADC must be disabled. */
/* Disable the ADC (if not already disabled) */
tmp_hal_status = ADC_Disable(hadc);
delay_uS(20); // added by me
/* Check if ADC is effectively disabled */
if (LL_ADC_IsEnabled(hadc->Instance) == 0UL)
{
/* Set ADC state */
ADC_STATE_CLR_SET(hadc->State,
HAL_ADC_STATE_REG_BUSY,
HAL_ADC_STATE_BUSY_INTERNAL);
/* Manage settings impacting calibration */
/* - Disable ADC mode auto power-off */
/* - Disable ADC DMA transfer request during calibration */
/* Note: Specificity of this STM32 series: Calibration factor is */
/* available in data register and also transferred by DMA. */
/* To not insert ADC calibration factor among ADC conversion data */
/* in array variable, DMA transfer must be disabled during */
/* calibration. */
backup_setting_cfgr1 = READ_BIT(hadc->Instance->CFGR1, ADC_CFGR1_DMAEN | ADC_CFGR1_DMACFG | ADC_CFGR1_AUTOFF);
CLEAR_BIT(hadc->Instance->CFGR1, ADC_CFGR1_DMAEN | ADC_CFGR1_DMACFG | ADC_CFGR1_AUTOFF);
/* ADC calibration procedure */
/* Note: Perform an averaging of 8 calibrations for optimized accuracy */
for (calibration_index = 0UL; calibration_index < 8UL; calibration_index++)
{
/* Start ADC calibration */
LL_ADC_StartCalibration(hadc->Instance);
delay_uS(20); // added by me
/* Wait for calibration completion */
while (LL_ADC_IsCalibrationOnGoing(hadc->Instance) != 0UL)
{
wait_loop_index++;
if (wait_loop_index >= ADC_CALIBRATION_TIMEOUT)
{
/* Update ADC state machine to error */
ADC_STATE_CLR_SET(hadc->State,
HAL_ADC_STATE_BUSY_INTERNAL,
HAL_ADC_STATE_ERROR_INTERNAL);
__HAL_UNLOCK(hadc);
return HAL_ERROR; // Code always return HAL_ERROR due to ADC_CALIBRATION_TIMEOUT
}
}
calibration_factor_accumulated += LL_ADC_GetCalibrationFactor(hadc->Instance);
}
/* Compute average */
calibration_factor_accumulated /= calibration_index;
/* Apply calibration factor (requires ADC enable and disable process) */
LL_ADC_Enable(hadc->Instance);
/* Case of ADC clocked at low frequency: Delay required between ADC enable and disable actions */
if (LL_ADC_GetClock(hadc->Instance) == LL_ADC_CLOCK_ASYNC)
{
adc_clk_async_presc = LL_ADC_GetCommonClock(__LL_ADC_COMMON_INSTANCE(hadc->Instance));
if (adc_clk_async_presc >= LL_ADC_CLOCK_ASYNC_DIV16)
{
/* Delay loop initialization and execution */
/* Delay depends on ADC clock prescaler: Compute ADC clock asynchronous prescaler to decimal format */
delay_cpu_cycles = (1UL << ((adc_clk_async_presc >> ADC_CCR_PRESC_Pos) - 3UL));
/* Divide variable by 2 to compensate partially CPU processing cycles */
delay_cpu_cycles >>= 1UL;
while (delay_cpu_cycles != 0UL)
{
delay_cpu_cycles--;
}
}
}
LL_ADC_SetCalibrationFactor(hadc->Instance, calibration_factor_accumulated);
LL_ADC_Disable(hadc->Instance);
/* Wait for ADC effectively disabled before changing configuration */
/* Get tick count */
tickstart = HAL_GetTick();
while (LL_ADC_IsEnabled(hadc->Instance) != 0UL)
{
if ((HAL_GetTick() - tickstart) > ADC_DISABLE_TIMEOUT)
{
/* New check to avoid false timeout detection in case of preemption */
if (LL_ADC_IsEnabled(hadc->Instance) != 0UL)
{
/* Update ADC state machine to error */
SET_BIT(hadc->State, HAL_ADC_STATE_ERROR_INTERNAL);
/* Set ADC error code to ADC peripheral internal error */
SET_BIT(hadc->ErrorCode, HAL_ADC_ERROR_INTERNAL);
return HAL_ERROR;
}
}
}
/* Restore configuration after calibration */
SET_BIT(hadc->Instance->CFGR1, backup_setting_cfgr1);
/* Set ADC state */
ADC_STATE_CLR_SET(hadc->State,
HAL_ADC_STATE_BUSY_INTERNAL,
HAL_ADC_STATE_READY);
}
else
{
SET_BIT(hadc->State, HAL_ADC_STATE_ERROR_INTERNAL);
/* Note: No need to update variable "tmp_hal_status" here: already set */
/* to state "HAL_ERROR" by function disabling the ADC. */
}
__HAL_UNLOCK(hadc);
return tmp_hal_status;
}
- Labels:
-
STM32G0 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-11-29 5:42 AM - edited ‎2024-11-29 5:43 AM
Hello @ogulcanyanik and welcome to the Community,
I will check your reported issue and update this thread accordingly.
An internal ticket ID 197378 is submitted to track and work on this request.
(PS: Ticket ID 197378 is an internal tracking number and is not accessible outside of ST).
Thanks
Imen
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-12-02 8:16 AM
hello @ogulcanyanik ,
Hello,
Your issue is not related to the post you mention, because occurring before.
Calibration procedure steps:
1. Perform calibration
1.1. with 8 loops (==> issue in the current post)
1.2. get calibration factors, compute average value
2. Set calibration factors
2.1. Enable ADC and wait for delay (==> issue you mention in previous post)
2.2. Set value in ADC register
Your issue seems that ADC automatic self-calibration does not reach completion: end of calibration flag does not raise (cf function LL_ADC_IsCalibrationOnGoing()).
Can you provide us more details:
- confirmation whether ADC bus clock is enabled (__HAL_RCC_ADC_CLK_ENABLE() setting RCC_APBENR2_ADCEN) ?
- what is the ADC kernel clock configuration:
- system: SysClk, HSI16, PLLPCLK and clock frequency ?
- ADC: HAL ADC init struct "ClockPrescaler" (or register CFGR2 content) ?
Best regards
Philippe