2020-06-05 10:02 AM
I have been using CubeMX to generate the HAL library files and noticed that it only generates for the newest version only. I also looked in to the GitHub repository and under the release there is only about 2 very recent versions of the libraries.
I want to get the distribution for the older versions and is there a way to get these? Thanks for the time
Solved! Go to Solution.
2020-06-05 03:54 PM
2020-06-05 10:39 AM
The CubeMX tool has historically been able to pull older versions into the repository.
The CubeF4, for example, download page used to allow you to pick the version to pull.
I've also posted mirrors in the past.
2020-06-05 11:05 AM
Could you please tell how I could pull older versions to the repository? I tried but there are only two or at most three most recent versions as the options.
2020-06-05 03:54 PM
2020-06-05 05:33 PM
Thank you so much