2023-12-16 05:28 AM
Hi ST Team,
Please suggest an camera part number which i can easily interface with the 32F746GDISCOVERY Board.
Kindly share the complete details.
Thanks & Regards,
Solved! Go to Solution.
2023-12-16 08:10 AM - edited 2023-12-16 08:27 AM
Hello again @Tajwar.Chandel
You can connect the board to the camera module using the 1 × 30 pin ZIF connector of each one of them.
For the camera module :
For the board :
for more details, refer to the UM1907 and the UM2779.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-12-16 05:56 AM
Hello @Tajwar.Chandel
You can use the B-CAMS-OMV camera module that is compatible with the STM32F4DIS-CAM camera module, so you can connect it to your STM32F746 Discovery board. The drivers of the B-CAMS-OMV can be found in the AI vision function pack.
Best Regards,
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-12-16 07:27 AM - edited 2023-12-16 07:59 AM
Can you please share any document for how to connect (interface) the B-CAMS-OMV camera module with 32F746GDISCOVERY Board. Hope you will help.
Tajwar
2023-12-16 07:47 AM
Hi,
Can you please share any document for how to connect (interface) the B-CAMS-OMV camera module with 32F746GDISCOVERY Board. Hope you will help.
Regards,
Tajwar
2023-12-16 08:10 AM - edited 2023-12-16 08:27 AM
Hello again @Tajwar.Chandel
You can connect the board to the camera module using the 1 × 30 pin ZIF connector of each one of them.
For the camera module :
For the board :
for more details, refer to the UM1907 and the UM2779.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-02-27 05:03 AM
Hello,
Please provide link to sample project for interfacing the 32F746GDISCOVERY - Discovery kit with camera module B-CAMS-OMV.
Regards,
Tajwar