cancel
Showing results for 
Search instead for 
Did you mean: 

What is value od HSE on nucleo L432KC?

oeliks
Senior

Hi, what is the value of HSE on nucleo nano board stm32l432kc ?

​https://www.st.com/en/evaluation-tools/nucleo-l432kc.html#overview

Future : 24MHz crystall

But when I initialize default settings in cubemx it sets HSE as 8 MHz.​

Cant find value of HSE on board in board User Manual.​

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
waclawek.jan
Super User

There is no HSE crystal mounted on Nucleo-32, and also there's no OSC_OUT pin on the 'L432KC, so you cannot use a crystal for HSE with that chip.

It still has OSC_IN, so you can use an external oscillator and HSE in Bypass mode. On the Nucleo-32, you would need to connect SB17 which connects the MCO output from the on-board STLink chip ('F103) to PA0 of the target i.e. 'L432KC, and the STLink's MCO output is 8MHz.

JW

View solution in original post

1 REPLY 1
waclawek.jan
Super User

There is no HSE crystal mounted on Nucleo-32, and also there's no OSC_OUT pin on the 'L432KC, so you cannot use a crystal for HSE with that chip.

It still has OSC_IN, so you can use an external oscillator and HSE in Bypass mode. On the Nucleo-32, you would need to connect SB17 which connects the MCO output from the on-board STLink chip ('F103) to PA0 of the target i.e. 'L432KC, and the STLink's MCO output is 8MHz.

JW