cancel
Showing results for 
Search instead for 
Did you mean: 

What is the purpose of the PMOS switch for VBAT-SYSTEM STM32L0x1 see AN4718

Oliver R.
Associate III

0693W00000Y85kLQAR.jpgAN4718 "How to design a V BAT system based on

STM32L0/L1 ..."

Case 1b, it is stated, quote:

"V DD /V DDA can also be switched to V BACKUP when STM32L0/STM32L1 MCU goes into STOP mode, to allow user to remove main supply in very safe way."

End quote.

Question: What does that mean "very safe" ?

What is the exact purpose of that PMOS switch ?

Is is to prevent the supercap current going to a battery pin ?

What is unsafe if not used ?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

OK, the remark "very safe" is perhaps a bit exaggerated, but it means that in the event of a main supply failure, no current flows from the backup supply into the main supply.

The PMOS allows for low-impedance and thus low-loss switching of the main supply. Since Schottky diodes have quite large reverse currents, it makes no sense to replace the PMOS with a Schottky.

Does it answer your question?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

3 REPLIES 3
Peter BENSCH
ST Employee

OK, the remark "very safe" is perhaps a bit exaggerated, but it means that in the event of a main supply failure, no current flows from the backup supply into the main supply.

The PMOS allows for low-impedance and thus low-loss switching of the main supply. Since Schottky diodes have quite large reverse currents, it makes no sense to replace the PMOS with a Schottky.

Does it answer your question?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Oliver R.
Associate III

I see. The main supply might be tied to ground, for instance, if broken, and that would shourtcut the supercap.

Thank you very much.

If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.