Skip to main content
Yoichi Shinoda
Senior
February 10, 2020
Solved

What does generally cause "ST-LINK device status: LOCKUP"?

  • February 10, 2020
  • 1 reply
  • 2101 views

I have an application for Nucleo-H7A3ZI-Q which causes "ST-LINK device status: LOCKUP" very early into an execution, as early as 2/3 of the way into initialized data section copy loop in startup.s.

STMicroelectronics ST-LINK GDB server. Version 5.2.3
Copyright (c) 2019, STMicroelectronics. All rights reserved.
 
Starting server with the following options:
 Persistent Mode : Enabled
 LogFile Name : debug.log
 Logging Level : 31
 Listen Port Number : 61234
 Status Refresh Delay : 15s
 Verbose Mode : Disabled
 SWD Debug : Enabled
 
Hardware watchpoint supported by the target 
SWD frequency = 4000 kHz
ST-LINK Firmware version : V3J0S0
Device ID: 0x480
PC: 0x8040eac
ST-LINK device status: HALT_MODE
ST-LINK detects target voltage = 3.26 V
ST-LINK device status: HALT_MODE
ST-LINK device initialization OK
Waiting for debugger connection...
Waiting for connection on port 61234...
Accepted connection on port 61234...
Debugger connected
Wrapping read detected. Addr: 0xfffffffe; Length: 4
TraceCaptureStart and SWV event set to APP_TRUE 
ST-LINK device status: LOCKUP
Enter STM32_AppReset() function 
NVIC_DFSR_REG = 0x00000009
NVIC_CFGFSR_REG = 0x00000000
XPSR = 0x01000000
Error! Failed to read target status 
Debugger connection lost.
Shutting down...

Client gdb gives E31 error and drops connection.

The same application, linked with data segment shifted few K bytes aft gives hard fault as early as few steps into the execution, immediately at the entry of the first bl call after sp initialization.

Well, the behavior is inconsistent, but the LOCKUP is really annoying.

What is the general cause of the LOCKUP behavior?

Any info would be appreciated.

EDIT

Some additional info

STLINK-V3 is flashed with V3J6M2, but the gdbserver is displaying "ST-LINK Firmware version : V3J0S0".

The application is over 512KB in flash size.

This topic has been closed for replies.
Best answer by Yoichi Shinoda

Self followup.

The issue seems to be resolved for Nucleo-H7A3ZI-Q with a combination of following software versions.

STLINK-V3 firmware

V3J6M2

(Now the gdbserver correctly reads the version.)

STLINK-gdbserver

5.4.0

Came with an installation of STM32CubeIDE 1.2.0 (or possibly 1.2.1; I came to notice the combination works after upgrading to 1.2.1)

Path to the working executable is as follows.

/Applications/STM32CubeIDE.app/Contents/Eclipse/plugins/com.st.stm32cube.ide.mcu.externaltools.stlink-gdb-server.macos64_1.1.0.201910081157/tools/bin/

1 reply

Yoichi Shinoda
Yoichi ShinodaAuthorBest answer
Senior
February 11, 2020

Self followup.

The issue seems to be resolved for Nucleo-H7A3ZI-Q with a combination of following software versions.

STLINK-V3 firmware

V3J6M2

(Now the gdbserver correctly reads the version.)

STLINK-gdbserver

5.4.0

Came with an installation of STM32CubeIDE 1.2.0 (or possibly 1.2.1; I came to notice the combination works after upgrading to 1.2.1)

Path to the working executable is as follows.

/Applications/STM32CubeIDE.app/Contents/Eclipse/plugins/com.st.stm32cube.ide.mcu.externaltools.stlink-gdb-server.macos64_1.1.0.201910081157/tools/bin/