cancel
Showing results for 
Search instead for 
Did you mean: 

Using AHPI7292S with STM32F7508-DK board

Sule_Akcay
Associate III

Hello
I want to use the AHPI7292S board with the STM32F7508-DK board.
Is AHPI7292S compatible with STM32F7508-DK board? Is there any study on this subject?

ddd.jpgWhatsApp Görsel 2024-05-03 saat 09.53.50_558aa0c2.jpg

1 REPLY 1

Perhaps there are manuals?

Perhaps there is workable software on the RPi and you can learn how at least one of the combinations works, and then pivot into the STM32 board and how you might wire the RPi and Arduino headers in a serviceable manner?

Not sure someone's going to provide you with a tutorial..

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..