cancel
Showing results for 
Search instead for 
Did you mean: 

STM32N6570-DK demo version update

Crigstar
Associate II

Hi, I have a STM32N6570-DK and I see that the available demo code is up to v1.3.0

How do I determine what version of code was shipped on the DK?

Is there a document that details how to upgrade the code if it’s needed?

STM32N6-OOBSTM32N6570-DK Out-of-the-box demo binary1.3.0

Thanks, Tony 

1 ACCEPTED SOLUTION

Accepted Solutions
AlexWEI
ST Employee

hi 

just use the cube programmer to upgrade the demo code. 

View solution in original post

6 REPLIES 6
TDK
Super User

You could download the firmware currently on the board and compare.

If you feel a post has answered your question, please click "Accept as Solution".

That’s a good idea. I’ll try to do that. I need to be careful as Download seems to send a file to the device and can’t see an Upload option. Still trying to get familiar with this.

TDK
Super User

Put in 1 MB as the size here and hit read. You may need to split it into multiple files.

TDK_0-1758025605487.png

Or, open the file you want to compare to and hit Verify here (don't hit Download or you'll lose what is on the chip):

TDK_1-1758025662649.png

 

If you feel a post has answered your question, please click "Accept as Solution".
Crigstar
Associate II

Thank you. I’ll try this but it will be a few weeks before I can get to it as I’ll be traveling.

AlexWEI
ST Employee

hi 

just use the cube programmer to upgrade the demo code. 

Hi, i ended up doing this but i was hoping that the demo indicated its version somewhere so i could avoid re-writing that same code to it.