cancel
Showing results for 
Search instead for 
Did you mean: 

STM32N6570-D: Is XSPI/OSPI for memory only, or also external peripherals?

MownishBugatha
Associate III

Does the STM32N6570-DK board support XSPI/OSPI interfaces for communication with external peripherals, or are these interfaces limited only to internal or external memory devices?

For example, if there is a Device that supports OSPI/XSPI for communication, is it possible to connect the STM32N6570-DK board to such a device to enable data exchange?

Could you please provide a clear explanation of the capabilities and practical use cases of the OSPI/XSPI interface on the STM32N6570-DK board?

12 REPLIES 12
MownishBugatha
Associate III

I want to Know the Answer for ASIC thats why i had unmarked the solution and Thanks a lot for your help. 
I will go through the document  attached.

Mikk Leini
Senior III

 @MownishBugatha maybe PSSI helps you out? It can clock in and out 8 or 16-bits at 100 MHz.

ok i will check that