cancel
Showing results for 
Search instead for 
Did you mean: 

STM32N6570-DK inconsistency with information in datasheets and parts used

Linas L
Senior II

I was looking at STM32N6, and it says it has 1G networking. Problem is, chip used is 100M. So how can they say that development kit supports 1G ?

LinasL_0-1742463756389.png
LAN8742A-CZ-TR chip used inside both devkits:

LinasL_1-1742463810845.png

Same goes to HR timer, it says on datasheet, it does support high resurrection timer, while no mention anywhere about it

LinasL_2-1742464078142.png

Is there nay more information regarding timer and does devkit support 1G ? I was hoping it could, since I could make IP camera or something similar.

 

5 REPLIES 5

@Linas L wrote:

I was looking at STM32N6, and it says it has 1G networking. Problem is, chip used is 100M. So how can they say that development kit supports 1G ?


Which development kit are you referring to?

Please give a link to where that screenshot came from.

https://www.st.com/en/evaluation-tools/stm32n6570-dk.html

Maybe in that case they say, chip itself does support it

LinasL_0-1742469247458.png

Both development kit uses same chip for networking

But they are clearly listing what is on the development board, since all features can't be 5inch LCD....

Sorry my bad, altium project looked similar, and both times I was able to open same one. RTL8211F-CG is actual chip on DK development kit, it does support 1000M.

So only high resolution timer left, no info on that one.

I've edited the post title to make that clear

TDK
Guru

> STM32N6570-DK

> it says on datasheet, it does support high resurrection timer

I see no hits for "high-resolution timer" in the datasheet of the board or the chip.

https://www.st.com/resource/en/datasheet/stm32n657x0.pdf

https://www.st.com/resource/en/data_brief/stm32n6570-dk.pdf

 

Perhaps it got removed. The chip doesn't have an HRTIM.

If you feel a post has answered your question, please click "Accept as Solution".