2024-12-14 04:05 AM
I am trying to run some basic tests on the STM32H7S78-DK discovery board.
I am having some trouble properly initializing the PSRAM (is this info available somewhere, what are the right settings?)
PSRAM is clocked at 200MHz, i copied settings from the available examples/bsp
I am having random errors, it looks like that sometimes the write is not executed
Most of the time like 99.99% of the case, everything works fine, but sometimes i read old data from the PSRAM, this mostly happens with 16 or 8 bit r/w but rarely also with 32 bit r/w
I have a test that writes the whole ram with some pattern then verifies it.
This happens in all combination of cache settings, but cache settings have a significant impact on the frequency of these errors (not clear why).
i'm logging the result, it looks something like this:
T32 for pattern 0fc52bc8 0 diff
T16 for pattern 00007118 0 diff
T8 for pattern 000000bb 0 diff
T32 for pattern 4fa30e48 0 diff
T16 for pattern 00005498 0 diff
T8 for pattern 0000003b 0 diff
T32 for pattern b4cf54f8 0 diff
T16 for pattern 00000e28
diff @ 0x91209040 : 0x54f8
diff @ 0x91209042 : 0xb4cf
diff @ 0x91209044 : 0x54f8
diff @ 0x91209046 : 0xb4cf
diff @ 0x91209048 : 0x54f8
diff @ 0x9120904a : 0xb4cf
diff @ 0x9120904c : 0x54f8
diff @ 0x9120904e : 0xb4cf
8 diff
For the last T16 test, i.e. overwrite the whole PSRAM content with 0x0e28, using 16bit access, there are 8 differences at 8 consecutive memory locations, where the write silently failed and the old data from the previous test is still present.
Any ideas or suggestions on how to debug this? I can not physically check/measure the lines between mcu and psram as they are not accessible, neither i have the equipment for it.
2024-12-15 10:38 PM
Hi,
I think you may reduce the work frequency to check whether such problem is still happened. another method is to change the clock phase to sample read data from PSRAM.
B.R.
2024-12-16 03:04 AM
i would not like to reduce clock frequency as it comes with performance hit, both the mcu and the psram is rated up to 200Mhz. I could play with various settings, but i will never know for sure, as i can't make physical measurements on the xspi lines.
Given that this is a fixed HW, designed and verified by ST, such parameters should be available that are optimal and are guaranteed to work (golden reference)