cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H747I-DISCO User Manual UM2411 incorrect

Andreas Bolsch
Lead II

The manual states two MX25QL512ABB8ESF-0SIT from

Macronix are fitted. That's wrong, there is no such device made by Macronix, in fact there are two MT25QL512ABB from Micron on the board (in accordance with the schematics).

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Amel NASRI
ST Employee

Hi @Andreas Bolsch​ ,

You are right, this is an error on UM2411 and it is reported internally to be fixed.

As you said, the correct one is MT25QL512ABB8ESF-0SIT (FBGA code = RW187) from Micron.

Thanks for bringing this error to our attention.

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.