2021-04-12 9:51 PM
Hi,
I have made a custom board that features a STM32F469NI MCU coupled with AS4C4M32S SDRAM.
Following are the SDRAM timing and register set information:
hsdram1.Instance = FMC_SDRAM_DEVICE;
/* hsdram1.Init */
hsdram1.Init.SDBank = FMC_SDRAM_BANK1;
hsdram1.Init.ColumnBitsNumber = FMC_SDRAM_COLUMN_BITS_NUM_8;
hsdram1.Init.RowBitsNumber = FMC_SDRAM_ROW_BITS_NUM_12;
hsdram1.Init.MemoryDataWidth = FMC_SDRAM_MEM_BUS_WIDTH_32;
hsdram1.Init.InternalBankNumber = FMC_SDRAM_INTERN_BANKS_NUM_4;
hsdram1.Init.CASLatency = FMC_SDRAM_CAS_LATENCY_3;
hsdram1.Init.WriteProtection = FMC_SDRAM_WRITE_PROTECTION_DISABLE;
hsdram1.Init.SDClockPeriod = FMC_SDRAM_CLOCK_PERIOD_2;
hsdram1.Init.ReadBurst = FMC_SDRAM_RBURST_DISABLE;
hsdram1.Init.ReadPipeDelay = FMC_SDRAM_RPIPE_DELAY_0;
/* SdramTiming */
SdramTiming.LoadToActiveDelay = 2;
SdramTiming.ExitSelfRefreshDelay = 7;
SdramTiming.SelfRefreshTime = 4;
SdramTiming.RowCycleDelay = 6;
SdramTiming.WriteRecoveryTime = 2;
SdramTiming.RPDelay = 2;
SdramTiming.RCDDelay = 2;
if (HAL_SDRAM_Init(&hsdram1, &SdramTiming) != HAL_OK)
{
Error_Handler( );
}
/* USER CODE BEGIN FMC_Init 2 */
FMC_SDRAM_CommandTypeDef cmd = { 0 };
cmd.CommandMode = FMC_SDRAM_CMD_CLK_ENABLE;
cmd.CommandTarget = FMC_SDRAM_CMD_TARGET_BANK1;
cmd.AutoRefreshNumber = 1;
cmd.ModeRegisterDefinition = 0;
HAL_SDRAM_SendCommand(&hsdram1, &cmd, 0xFFFF);
HAL_Delay(100);
cmd.CommandMode = FMC_SDRAM_CMD_PALL;
cmd.CommandTarget = FMC_SDRAM_CMD_TARGET_BANK1;
cmd.AutoRefreshNumber = 1;
cmd.ModeRegisterDefinition = 0;
HAL_SDRAM_SendCommand(&hsdram1, &cmd, 0xFFFF);
cmd.CommandMode = FMC_SDRAM_CMD_AUTOREFRESH_MODE;
cmd.CommandTarget = FMC_SDRAM_CMD_TARGET_BANK1;
cmd.AutoRefreshNumber = 8;
cmd.ModeRegisterDefinition = 0;
HAL_SDRAM_SendCommand(&hsdram1, &cmd, 0xFFFF);
cmd.CommandMode = FMC_SDRAM_CMD_LOAD_MODE;
cmd.CommandTarget = FMC_SDRAM_CMD_TARGET_BANK1;
cmd.AutoRefreshNumber = 1;
cmd.ModeRegisterDefinition = (uint32_t) 0x230; //also tried 0x231
HAL_SDRAM_SendCommand(&hsdram1, &cmd, 0xFFFF);
//Setup SDRAM Refresh Timer Register with the delay between refresh cycles of the SDRAM, this is SDRAM specific.
HAL_SDRAM_ProgramRefreshRate(&hsdram1, 1404); //Tried 1386This same code works when running on a STM32F469-I DISCOVERY Board but fails when It is run on my custom carrier board.
On my board, whenever I write to any SDRAM address, only the first byte is READ/WRITTEN to, for example when I write 0x00 to address 0xC0000000, the data at that address when monitored under debugging contains 0x48129100 i.e first 3 BYTES are random garbage and only the last byte is written correctly(0x00), and suppose If i write 0xAA to the same address the data there when monitored contains the value 0x481291AA.
This is true to every address that I read/write to/from the external SDRAM.
Only the last byte is written/read.
The custom board schematic and PCB layout is identical to the STM32F469-I DISCO board.
Only difference is the RAM chip which instead of being MICRON one is Alliance Memory's AS4C4M32S .
What can be the issue of such a problem?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.