cancel
Showing results for 
Search instead for 
Did you mean: 

STLINK V3 ISOL - what speed should it run at?

PHolt.1
Senior III

It fails at 24MHz, but mostly works at 8MHz. Is there a spec on it somewhere?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

Chart says SWD 12 MHz

"Table 19. Achievable maximal performance with STLINK-V3SET on different channels"

https://www.st.com/resource/en/user_manual/dm00526767-stlinkv3set-debuggerprogrammer-for-stm8-and-stm32-stmicroelectronics.pdf

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

View solution in original post

3 REPLIES 3

Chart says SWD 12 MHz

"Table 19. Achievable maximal performance with STLINK-V3SET on different channels"

https://www.st.com/resource/en/user_manual/dm00526767-stlinkv3set-debuggerprogrammer-for-stm8-and-stm32-stmicroelectronics.pdf

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
PHolt.1
Senior III

OK - 8MHz. Many thanks.

Curiously that table states 16MHz for the SWV, while Cube IDE supports a max speed of 2MHz. Getting this to go faster would be useful because it affects the execution speed of SWV ITM debug output; you want maximum speed on that.

PHolt.1
Senior III

I did some tests, on straight code loading, no debugging etc, and the ISOL board bombs out around 18MHz. This is probably cabling dependent.

Note that there is a weird problem with the connector usage

https://peter-ftp.co.uk/screenshots/20210510393155911.jpg