cancel
Showing results for 
Search instead for 
Did you mean: 

stm32cubeide version 1.19.0 (Build: 25607_20250703_0 ) debuging problem with the stm32F429ZI_disc1

mkosu.2
Associate

Dear Sir/Madam ,

 

I have imported BSP package for the stm32F429zi-disc1 board to the stm32cube ide and connected to the disc1 board over STLink Interface and then tried to start debugging ; but I could not download the executable file and I have got the following error. I have also upgraded the firmware of the STLink on the Disc1 board to the latest one. But I have got the same result. Firmware version of the board is V2J46M33 . Please help me on this issue.

 

Remark : Please also note that I was able to download the same hex file to the board using stm32cubeprogrammer version 2.20.

 

 

Error in final launch sequence:

 

Failed to execute MI command:

load C:\\Users\\Lenovo\\STM32Cube\\Repository\\STM32Cube_FW_F4_V1.28.2\\Projects\\STM32F429I-Discovery\\Examples\\BSP\\STM32CubeIDE\\Discovery_Debug\\BSP.elf

 

Error message from debugger back end:

Error finishing flash operation

Failed to execute MI command:

load C:\\Users\\Lenovo\\STM32Cube\\Repository\\STM32Cube_FW_F4_V1.28.2\\Projects\\STM32F429I-Discovery\\Examples\\BSP\\STM32CubeIDE\\Discovery_Debug\\BSP.elf

 

Error message from debugger back end:

Error finishing flash operation

Failed to execute MI command:

load C:\\Users\\Lenovo\\STM32Cube\\Repository\\STM32Cube_FW_F4_V1.28.2\\Projects\\STM32F429I-Discovery\\Examples\\BSP\\STM32CubeIDE\\Discovery_Debug\\BSP.elf

 

Error message from debugger back end:

Error finishing flash operation

Error finishing flash operation

0 REPLIES 0