2024-04-18 5:00 AM
Hello,
I would like to interface STM32U5G9 with SD Card. Looking at SensorTileBox.Pro schematic, I see that an SD Card Driver (st6g3244mebjr) is placed in the middle. What is the added value in using it?
Thank you
Solved! Go to Solution.
2024-04-18 6:43 AM
The ST6G3244MEBJR (U16) is used as a level translator from 1.8V to 3.0V.
Does it answer your question?
Regards
/Peter
2024-04-18 6:43 AM
The ST6G3244MEBJR (U16) is used as a level translator from 1.8V to 3.0V.
Does it answer your question?
Regards
/Peter
2024-04-18 6:50 AM - edited 2024-04-18 7:17 AM
That's ok.
I double checked the topic and, as the SD Card initial communication voltage level is at 3.3 V (only when switching to UHS-I changes to 1.8 V), we need for a certain initial time to shift communication to 3.3V. In SensorTileBox.Pro the STM32U5 is powered at 1.8 V. I hoped that the voltage level change could be managed directly by STM32U5, but it is stated the an external voltage level translator is needed.
Thank you