2024-10-24 11:09 PM
What is the highest value series resistor which can be put into the ICSP Vapp pin a design?
It being connected to VDD and presenting a risk of harm if connected wrongly.
I can spend time testing this but would prefer to know if this has a definite value.
2024-10-30 3:36 AM
I tested 5k, errors only. 2.5k seemed OK, and I only need 330R so that will do.
I'll leave this open for further comments. My programmer is the ST-LINK V2
2024-10-30 3:57 AM
@CGadg wrote:My programmer is the ST-LINK V2
Genuine, or clone?
2024-10-30 4:06 AM
It's a genuine one
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.