cancel
Showing results for 
Search instead for 
Did you mean: 

ST-Link V2 Driver for Win11arm on Parallels on MacMini M4

Andreas8882
Associate II

I'm searching for the ST-Link V2 driver to use on win11arm running on parallels on a MacMini M4.

The CubeProgrammer 2.19 directly installed on M4 macOS is properly working with the ST-Link-V2 or some nucleo boards for only programming use. But because I use IAR embedded Workbench for development and debugging I must have a working solution on the Win11arm platform (parallels) of my M4 machine. The driver of the CubeProgrammer 2.19 installation on win11arm platform don't work (windows device manager show: no driver installed). Is there anywhere a stable working solution from STM?

0 REPLIES 0