cancel
Showing results for 
Search instead for 
Did you mean: 

RTC precision on H573I-DK board

emd64
Associate

Hi,

I'm running test on the Discovery board H573I-DK.

On a 24 hours period, I measure a 340 ppm precision that is far from the 20 ppm of the LSE Quartz.

Is it normal ?

3 REPLIES 3
Uwe Bonnes
Chief

Did the board run to slow? If  yes, was the board running continious or did resets happen as caused by loading a new programm. It is quit easy to stop the RTC for some short period during programm startup  while the startup code checks the status of the RTC.

mƎALLEm
ST Employee

Hello @emd64 and welcome to the community,

Refer also to this knowledge base: How to calibrate the STM32's real-time clock (RTC)

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
waclawek.jan
Super User

> I'm running test

What test?

> I measure a 340 ppm precision

How do you measure that?

Read out and check/post content of RCC_BDCR and RTC registers.

Also, as @Uwe Bonnes said above, Cube/HAL used to (and may still do?) cause RTC to be delayed upon each reset.

JW