2024-07-16 5:53 AM
I am currently Attempting to get Lorawan Fuota working for a duel core system. It is without question connected to my device and it seems to work fine. On the software end, attempting to use build.bat appears to work fine as well. But whenever I attempt to use the program.bat file in a similar manner I get:
###########################################
# 0- Set all global variables
###########################################
###########################################
# 1- Disable security
###########################################
###########################################
# 1- Disable security
###########################################
RDP: Read Out protection Level 1
Error: Command write -ob RDP=0xBB Failed PS C:\Users\Intern\STM32Cube\Repository\STM32Cube_FW_WL_V1.3.0\Projects\NUCLEO-WL55JC\Applications\LoRaWAN_FUOTA_DualCore\Scripts\STM32CubeIDE>
Is this an error on windows powershell? Or is there something wrong with the file itself? I am following the tutorial made by the stm32 channel: https://www.youtube.com/watch?v=PQVXhu8520o to the letter so I'm not sure what I'm doing wrong. My best guess is that for whatever reason windows powershell is not connecting to my stm32 device properly. As this same error is received whether or not the device is connected.
2024-07-16 7:42 AM
Hello @Confused_Intern and welcome to the ST Community :smiling_face_with_smiling_eyes:.
I've tested this on my side, and it works very well will the board is connected to my PC. I suggest you change the communication USB cables that you are using. Or check that the board is working fine.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-07-16 10:57 AM
I downloaded example onto a new computer (Which has stm32 installed), navigated to the repository, used a new USB and new end device and it still got the same error. Is there a specific version of windows powershell I'm supposed to use?
2024-07-16 10:59 AM
Does the end device need to be entirely new fresh out of the box?
2024-07-16 11:41 AM
You have just to ensure it is working fine.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.