cancel
Showing results for 
Search instead for 
Did you mean: 

"Error: Initializing the option bytes failed" when trying to connect with device in dfu mode

Snulu.1
Associate

Hi all,

I'm using STM32F767 Microcontroller.

For flashing FW to the controller I'm using STM32CubeProgrammer through USB DFU mode.

By making the BOOT pin high, I tried to connect the device with programmer through USB.

Then I observed the error screen pop-up shoeing "error: initializing option bytes failed".

This is not happening in all PCBs. It happened only in some PCBs.

Attached the screenshot for your reference.

Can anyone help me in knowing why this error message is coming and how to fix this.

1 REPLY 1
FBL
ST Employee

Hello @Snulu.1​,

I was wondering if you are facing the same issue. Could you try to check your boot configuration using AN4661 section 4 Boot configuration. Also verify your boot pin connection in the following section.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.