2025-02-26 7:03 AM
Hello,
Does someone have information, project, whatever that can help me understand how do the Queues and Nodes work and interact with each other?
My STM32 has two ADCs, ADC1 & ADC4, and i want to trigger both of them to read values comming from multiple potentiomenters with a timer configured in output compare mode.
The problem is that i have to configure a linkedlist with a Queue and a Node and if i configure two nodes the values of the ADCs seen through the live expression get stuck at 0.
Any help is welcomed ...