cancel
Showing results for 
Search instead for 
Did you mean: 

Putty not receiving Data from NUCLEO-F303ZE

Athandile
Associate II

Title edited to be clear that this is on a NUCLEO-F303ZE board.


Hello all.

I'm trying to write a simple message via UART to Putty using stm32f303ze microcontroller. I'm using USART2, via ST-link. All the configurations have been confirmed (baud rate, COM port, bits, etc.) And they are right. I even tried using the STM32 Cube IDE Terminal with no luck. Now I'm not sure if the problem is the UART I'm using, or I'm doing something wrong in the code.

Also I'm not sure about the UART that support VCP in STM32F303ZE microcontrollers. However I tried all the USART, and the were no response in the Terminals.

 

Below is the simple message I'm trying to send and the full code.

/* USER CODE BEGIN Header */

/**

  ******************************************************************************

  * @file : main.c

  * @brief : Main program body

  ******************************************************************************

  * @attention

  *

  * Copyright (c) 2025 STMicroelectronics.

  * All rights reserved.

  *

  * This software is licensed under terms that can be found in the LICENSE file

  * in the root directory of this software component.

  * If no LICENSE file comes with this software, it is provided AS-IS.

  *

  ******************************************************************************

  */

/* USER CODE END Header */

/* Includes ------------------------------------------------------------------*/

#include "main.h"



/* Private includes ----------------------------------------------------------*/

/* USER CODE BEGIN Includes */

#include <string.h>





/* USER CODE END Includes */



/* Private typedef -----------------------------------------------------------*/

/* USER CODE BEGIN PTD */



/* USER CODE END PTD */



/* Private define ------------------------------------------------------------*/

/* USER CODE BEGIN PD */



/* USER CODE END PD */



/* Private macro -------------------------------------------------------------*/

/* USER CODE BEGIN PM */



/* USER CODE END PM */



/* Private variables ---------------------------------------------------------*/

UART_HandleTypeDef huart2;



/* USER CODE BEGIN PV */



/* USER CODE END PV */



/* Private function prototypes -----------------------------------------------*/

void SystemClock_Config(void);

static void MX_GPIO_Init(void);

static void MX_USART2_UART_Init(void);

/* USER CODE BEGIN PFP */



/* USER CODE END PFP */



/* Private user code ---------------------------------------------------------*/

/* USER CODE BEGIN 0 */







/* USER CODE END 0 */



/**

  * @brief The application entry point.

  * @retval int

  */

int main(void)

{



  /* USER CODE BEGIN 1 */



  /* USER CODE END 1 */



  /* MCU Configuration--------------------------------------------------------*/



  /* Reset of all peripherals, Initializes the Flash interface and the Systick. */

  HAL_Init();



  /* USER CODE BEGIN Init */



  /* USER CODE END Init */



  /* Configure the system clock */

  SystemClock_Config();



  /* USER CODE BEGIN SysInit */



  /* USER CODE END SysInit */



  /* Initialize all configured peripherals */

  MX_GPIO_Init();

  MX_USART2_UART_Init();

  /* USER CODE BEGIN 2 */





  /* USER CODE END 2 */



  /* Infinite loop */

  /* USER CODE BEGIN WHILE */

  while (1)

  {

    /* USER CODE END WHILE */



    /* USER CODE BEGIN 3 */

  char msg[] = "UART test OK\r\n";



  HAL_UART_Transmit(&huart2, (uint8_t*)msg, strlen(msg), HAL_MAX_DELAY);

  HAL_Delay(1000);



  }

  /* USER CODE END 3 */

}



/**

  * @brief System Clock Configuration

  * @retval None

  */

void SystemClock_Config(void)

{

  RCC_OscInitTypeDef RCC_OscInitStruct = {0};

  RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

  RCC_PeriphCLKInitTypeDef PeriphClkInit = {0};



  /** Initializes the RCC Oscillators according to the specified parameters

  * in the RCC_OscInitTypeDef structure.

  */

  RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;

  RCC_OscInitStruct.HSIState = RCC_HSI_ON;

  RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;

  RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;

  if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)

  {

    Error_Handler();

  }



  /** Initializes the CPU, AHB and APB buses clocks

  */

  RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK

                              |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;

  RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI;

  RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;

  RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;

  RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;



  if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK)

  {

    Error_Handler();

  }

  PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_USART2;

  PeriphClkInit.Usart2ClockSelection = RCC_USART2CLKSOURCE_PCLK1;

  if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)

  {

    Error_Handler();

  }

}



/**

  * @brief USART2 Initialization Function

  *  None

  * @retval None

  */

static void MX_USART2_UART_Init(void)

{



  /* USER CODE BEGIN USART2_Init 0 */



  /* USER CODE END USART2_Init 0 */



  /* USER CODE BEGIN USART2_Init 1 */



  /* USER CODE END USART2_Init 1 */

  huart2.Instance = USART2;

  huart2.Init.BaudRate = 115200;

  huart2.Init.WordLength = UART_WORDLENGTH_8B;

  huart2.Init.StopBits = UART_STOPBITS_1;

  huart2.Init.Parity = UART_PARITY_NONE;

  huart2.Init.Mode = UART_MODE_TX_RX;

  huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE;

  huart2.Init.OverSampling = UART_OVERSAMPLING_16;

  huart2.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;

  huart2.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;

  if (HAL_UART_Init(&huart2) != HAL_OK)

  {

    Error_Handler();

  }

  /* USER CODE BEGIN USART2_Init 2 */



  /* USER CODE END USART2_Init 2 */



}



/**

  * @brief GPIO Initialization Function

  *  None

  * @retval None

  */

static void MX_GPIO_Init(void)

{

  /* USER CODE BEGIN MX_GPIO_Init_1 */



  /* USER CODE END MX_GPIO_Init_1 */



  /* GPIO Ports Clock Enable */

  __HAL_RCC_GPIOA_CLK_ENABLE();



  /* USER CODE BEGIN MX_GPIO_Init_2 */



  /* USER CODE END MX_GPIO_Init_2 */

}



/* USER CODE BEGIN 4 */



/* USER CODE END 4 */



/**

  * @brief This function is executed in case of error occurrence.

  * @retval None

  */

void Error_Handler(void)

{

  /* USER CODE BEGIN Error_Handler_Debug */

  /* User can add his own implementation to report the HAL error return state */

  __disable_irq();

  while (1)

  {

  }

  /* USER CODE END Error_Handler_Debug */

}

#ifdef USE_FULL_ASSERT

/**

  * @brief Reports the name of the source file and the source line number

  * where the assert_param error has occurred.

  *  file: pointer to the source file name

  *  line: assert_param error line source number

  * @retval None

  */

void assert_failed(uint8_t *file, uint32_t line)

{

  /* USER CODE BEGIN 6 */

  /* User can add his own implementation to report the file name and line number,

     ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */

  /* USER CODE END 6 */

}

#endif /* USE_FULL_ASSERT */

Post edited by ST moderator to be inline with the community rules for the code sharing. In next time please use </> button to paste your code. Please read this post: How to insert source code.

 

13 REPLIES 13

Thank you so much, it’s working now.

I noticed that PB10 and PE15 were automatically configured by STM32CubeIDE when I enabled the USART during configuration. I saw in the datasheet that multiple pins are associated with each U(S)ART, but I’m struggling to understand how to determine which pins to use and when.

The IDE automatically assigns pins linked to a specific register, but I’d like to understand the logic or criteria behind this process. How am I suppose to know that USART is attached to PD8 and PD9 while the IDE enabled the other pins? I’ve attached some images from one datasheet for your reference.

Thank you once again for your guidance and support.Screenshot 2025-10-28 010332.pngScreenshot 2025-10-28 010230.png

Thank you so much, it’s working now.

I noticed that PB10 and PE15 were automatically configured by STM32CubeIDE when I enabled the USART during configuration. I saw in the datasheet that multiple pins are associated with each U(S)ART, but I’m struggling to understand how to determine which pins to use and when.

The IDE automatically assigns pins linked to a specific register, but I’d like to understand the logic or criteria behind this process. How am I suppose to know that USART is attached to PD8 and PD9 while the IDE enabled the other pins? I’ve attached some images from one datasheet for your reference.

Thank you once again for your guidance and support.Screenshot 2025-10-28 010230.pngScreenshot 2025-10-28 010332.png

Note that everyone can see all posts - there's no need to repeat your reply multiple times.

You can mention multiple people in one post using '@'

 


@Athandile wrote:

I’m struggling to understand how to determine which pins to use and when.


To use the VCP, you must use whichever pins are connected to the VCP !

Again, look in the User Manual (and/or the schematics) for your board - they will tell you which pins are physically connected to the VCP.

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

> How am I suppose to know that USART is attached to PD8 and PD9 while the IDE enabled the other pins?

Several ways:

  • Several posts here told you.
  • The board user manual tells you.
  • The schematic of the board will show which pins are connected.
  • A CubeMX project generated for that board will have the correct pins connected.
If you feel a post has answered your question, please click "Accept as Solution".