2025-04-18 8:40 AM - last edited on 2025-04-18 10:45 AM by STTwo-32
If I realize it is true, is it needed to solder SB12 in NUCLEO-WBA52CG board for using SWO as ITM_SendChar in printf debug?
Thank you for helping!
2025-04-18 10:51 AM
Hello @Arielu and welcome to the ST Community.
The SB12 need to be soldered if you are going to use GPIO32 (Pin 10 of the CN4) as SWO.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.