cancel
Showing results for 
Search instead for 
Did you mean: 

NUCLEO-G071RB catch 22 - PA14 set to GPIO input

pdornier1
Visitor

I flashed firmware that sets. Now STM32Cubeprogrammer refuses to connect to the STLINK portion.

How to recover from this / debrick the boards ? I tried pulling up PA14 / boot0 pin with a pull-up to CN7 pin 7, but no such luck...

2 REPLIES 2
Andrew Neil
Super User

Having the ST-Link connect under hardware reset should do it.

 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

Nope...

12:42:17 : UR connection mode is defined with the HWrst reset mode
12:42:22 : UR connection mode is defined with the HWrst reset mode
12:42:22 : ST-LINK error (DEV_USB_COMM_ERR)
12:42:22 : Error: Problem occured while trying to connect

Serial console through STLINK _is_ working, and shows my startup message, so the USB connection is good.

pdornier1_0-1762429700364.png