2024-06-18 8:21 AM
Hi,
I'm going to say that this is a really nooby question, however I cannot find the answer anywhere.
Background, I'm using a nucleo F103RB, and I've programmed it using CubeIDE. I can connect the board, debug and  run the program fine. The board is powered via Vin at the correct voltages, with JP1 disconnected and JP5 set to E5V.
I need to be able to run this program immediately after the board powers on, without a USB connection. How do I upload a release build of my program to it, because whenever I try using cubeprogrammer, it doesn't run the program after it has restarted. When I've tried dragging and dropping the .elf file in, it's given me a write error.
Thanks in advance for your help,
P
Solved! Go to Solution.
2024-06-19 9:15 AM
Everything is powered correctly, the board lights up but has the ST-Link waiting for connection. The clock is set up to come from the ST-Link. My code runs straight from a while loop in main after the peripheral initialisation.
I program the board via usb, set the jumpers to run via external power, then power it via my circuitry without usb connection, the board powers on, but does nothing except wait for connection. I plug USB back in and run the release code from cube IDE. The board powers and runs as expected.
If I check the storage in cube programmer it has the correct program in it.
Thanks
P
2024-06-19 10:05 AM
Does the ST-Link get powered-up in that state?
2024-06-20 2:09 AM
Yeah the ST-Link comes on and flashes Red while waiting for connection
2024-06-20 2:23 AM
Have you checked for a clock signal at the Target MCU?
2024-06-20 2:55 AM
yeah it's getting a signal, I don't know if it's correct or not though
2024-06-20 3:17 AM
Is it the same in both the working & non-working cases?
2024-06-20 3:22 AM
Yeah
2024-06-20 3:53 AM
I've just tried running it by dragging the .bin into the drive. This also didn't work. The only time it works is when it's been uploaded via STM32CubeIDE by pressing run. Any other time it is powered on, it doesn't run the code. Is there some sort of code CubeIDE sends to tell it to run, or something I need to put into my code to tell it to run on power on?
Thanks
2024-06-24 2:18 AM
I've done some more testing, I need to trigger a reset after power on, best way of doing this is with a POR chip
2025-02-21 3:01 AM - edited 2025-02-21 3:33 AM
Hello I am pretty new to the stm32 board and i am having exact same issue my jp1 pin is disconnected and i cannot find the jp5 pin though, so basically how do I trigger reset, do i just press the black button on the board? I would be grateful if you could provide pictures of the board as well
UPDATE: I found the jp5 pin header after reading the data sheet it is the 3 pins below reset button.
to elaborate the issue more i have a code which reads analog input and then send a fitting pwm signal i have tested the code in the debugger and it works fine but as soon as I run the code(upload it i am using stm32cubeide) it works fine as well but after a power cycle i see no signs that code is executing. the power led keeps blinking i am powering the controller via Vin i have grounded and all installed correctly