cancel
Showing results for 
Search instead for 
Did you mean: 

Need MT25QL512A_STM32769I-EVAL.stldr project source in TrueSTUDIO for ST-LINK utility

Ajith P V
Associate II
Posted on May 15, 2017 at 11:54

Hi,

Currently, we are using a STM32F769 based custom platform with S25FL512SAGMFIG11 (from Cypress) as QSPI external flash.

The flash which used in STM32769I-EVAL platform is 

MT25QL512ABA8ESF-0SIT and I can easily select the external flash from ST-Link utility since, this is a predefined configuration. Now, I have referred Section '3.9 Developing customized loaders for external memory' from STM32 ST-LINK utility software description (UM0892 User manual) and found that, only 2 or 3 flash support source is shown with TrueSTUDIO configuration.

Since, my platform is very close to the 

STM32769I-EVAL, I would like to get the MT25QL512A_STM32769I-EVAL.stldr project source in TrueSTUDIO for ST-LINK utility. So that, I can easily change the External flash configurations alone and make it work on our platform.

PS: The examples sources are for pretty different MCUs and I need to change the entire source just to make the external flash ready.

Thank you in advance,

Ajith P V

#project-source #stm32 #stlink #truestudio #configuration #stm32f769i-eval #external-flash
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Job Menue
Associate II
Posted on October 05, 2017 at 15:54

I have the same question, but then with the source code for the MT25QL512A_STM32756G-EVAL.stldr.

I don't understand why ST only includes two types of MCU's in their examples for external loaders. I'm having a lot of difficulties with mine.