MCP2515 in Interrupt mode using STM32WL
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2024-06-17 7:54 AM
Hi all,
I'm using MCP2515 for a CAN application in the NUCLEO STM32WL board. I've managed to get it to work in pulling mode, however, I want to use interrupt mode.
For what I looked, I just have to enable the MCP interrupt pin in EXTI mode in cubeMX, but the MCP interrupt pin that I set (PA0) is already set as the BUT1 pin (on board button). I didn't change the configurations, only set in the callback to activate if occurs the rising edge of BUT1_Pin (tried with falling edge too).
It didn't work, but I don't know if I have to configure something more, or the fact that the pin is shared with the button changes something and it could be the problem.
Any insights will be helpfull.
- Labels:
-
ST boards
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2024-06-26 7:55 PM
So either enable pullups for the stm32 pin or connect pullups. Datasheet is your best friend for the register programming. Good luck

- « Previous
-
- 1
- 2
- Next »