cancel
Showing results for 
Search instead for 
Did you mean: 

Low Peak to peak voltage on my PWM signal

yellow
Associate

Hello I am currently doing a project where I am using a STM32Nucleo-C092RC to generate a PWM signal the only problem is that my peak to peak voltege is only 160 mV. Is there any way to fix it so it is or is my board broken?

3 REPLIES 3
TDK
Super User

What pin are you using? Don't use a pin that is already in use.

https://www.st.com/resource/en/schematic_pack/mb2046-c092rc-b03-schematic.pdf

 

Ensure pin speed is set to VERY HIGH.

 

Show how you are measuring the peak-peak voltage.

If you feel a post has answered your question, please click "Accept as Solution".
Andrew Neil
Super User

Welcome to the forum.

As @TDK said, you need to give more information - see:

How to write your question to maximize your chances to find a solution

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
Ozone
Principal III

Configuring a GPIO as open-drain without attaching a resistor and measuring with a multimeter / scope would produce similiar results.