2025-08-08 6:46 AM
Hello,
I’m working on a FOC (Field Oriented Control) project to drive a PMSM (Permanent Magnet Synchronous Motor). I’m looking for an official STMicroelectronics development board that includes the following features:
STM32-based microcontroller
Supports resolver and encoder input (preferably both)
Gate driver outputs for external power stage (or integrated solution is fine)
Fully compatible with FOC-based motor control
Does ST offer such a motor control/inverter board?
Please recommend any official ST hardware that fits these criteria.
2025-08-20 2:02 AM
Hello @htuncer14 ,
You can download the MCDSK tool from this link.
Refer to the Release note available through Workbench tool > About > Documentations for the list of supported devices and boards. This list also includes inverter boards.
Hall sensors and Quadrature Encoder sensors are supported for speed sensing.