cancel
Showing results for 
Search instead for 
Did you mean: 

Issue porting BLE functionality on NUCLEO-WB09KE board, custom project

matthurst
Associate

Software: STM32CubeIDE v1.18.0, STM32CubeMX v6.14.0, STM32CubeProgrammer v2.17.0

Hardware: NUCLEO-WB09KE

 

Hello,

I am trying to observe Bluetooth functionality on a NUCLEO-WB09KE board. I have run the p2p_server example for the board unaltered, and it works perfectly. The device is discoverable using a Bluetooth scanner on my phone. However, when I try to copy the .ioc settings and BLE configuration to a custom project (no changes have been made to the .ioc file), it is no longer discoverable. Even when I copy and paste the .ioc file and create the new project from it, it still is not discoverable. I have debugged to verify that I am not ending up in an error handler, and I am not. APPE_Process is running. The only difference is that I am creating a new project and trying as opposed to copying the example from ST. I want to be able to observe BLE functionality in a custom project. Any help here would be appreciated!


Matt H.

1 REPLY 1
Billy OWEN
ST Employee

Hi @matthurst 

 

This post has been escalated to the ST Online Support Team for additional assistance.  We'll contact you directly.

 

Regards,

Billy