2020-09-16 7:38 AM
2020-09-16 9:14 AM
Yes and yes. That clock would be HSE bypass mode. Doesnt have to be MCO, it could also just be a timer.
2020-09-16 9:18 AM
Yes, this is how many of the NUCLEO/DISCO boards work, and connect with the ST-LINK STM32F103 device.
You could also share a common clock between units, which might actually be preferable.
You would need to drive NRST independently, the GPIO would need to be in open-drain mode as the pin is bidirectional, the STM32 can reset itself (POR, WDG, etc). Driving the NRST pin high with a push-pull driver will likely result in undesirable operation.