2019-11-19 8:18 AM
Hello,
Iam using STM32H743 Nucleo board.
Suddenly The Red LED (Over current LED) is glowing in my Micro controller. I have cheked all the connections properly there is no short circuit in it.
Because of this i cant able to load the Program in it It is showing Target Not Found Error.
When i Checked the Data Sheet . it is written like if the board power consumption in the USB Exceeds 500 mA Then the LED will glow it seems .
i am powering with my laptop till today morning it was working fine. May i know what is the cause
Kindly give me the solution to get out of it.it will be very helpfull
@Community member
Please find the attached pic and data sheets
Regards,
Muthukumar Ganesan
Solved! Go to Solution.
2019-11-20 1:37 PM
Could be an issue with the port or cable.
Or that you've shorted something out, or damaged the board.
There is no need to attach manuals, a web link will suffice.
You could try connecting the BOOT pin to VDD if you think it is something related to code you recently uploaded.
2019-11-20 1:37 PM
Could be an issue with the port or cable.
Or that you've shorted something out, or damaged the board.
There is no need to attach manuals, a web link will suffice.
You could try connecting the BOOT pin to VDD if you think it is something related to code you recently uploaded.
2019-11-22 7:13 AM
Thank you so much for Replying. and thank you so much for pointing me the cause . Something got Short that is the Problem.