2022-07-16 4:41 AM
I am designing a line-following robot that also avoids various obstacles (two digital infrared (IR) sensors), but I am a bit confused with my schematic since I am a beginner in electronics, and that is why I would like to know if my schematic is correct and if it is going to work. The robot's board utilizes two TB6612FNG BY TOSHIBA dual motor drivers modified in order to control one motor instead of two hence my robot has two individual motors. Furthermore, it uses the STM32F103C8T6 MCU. You can see details of the schematic in the image and the PDF file as well. Constructive criticism is accepted! Any answer is greatly appreciated!!!
Solved! Go to Solution.
2022-07-16 7:02 AM
I didn't review all the schematics. Only some remarks:
My 2 cents...
2022-07-16 7:02 AM
I didn't review all the schematics. Only some remarks:
My 2 cents...
2022-07-16 9:31 AM
And maybe FT232 isnt required. What is purpose?