cancel
Showing results for 
Search instead for 
Did you mean: 

How to use ST-Link Server?

Josh Yu
Associate II
Posted on April 09, 2018 at 08:16

Hi all,

I installed the ST-Link Server and after starting it, it opens up the default port 7184 on the local machine. But I have no idea how to interact with it. It's not a HTTP server, because using it over a browser doesn't show anything. When I connect to it over telnet, anything I type in and enter it says '0 unknown_command'. Is there a manual of some sort?

Thanks!

#stlink
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Till Rachow
Associate III
Posted on May 08, 2018 at 14:47

Same question here.. How to use it on a mac? Can't even find an application icon after installation..

Till Rachow
Associate III
Posted on May 08, 2018 at 16:02

So i just realized after running the installer, i got a new option in eclipse debug configurations under Debugger.

Here you can activate the st link server and chose from your different st links..