cancel
Showing results for 
Search instead for 
Did you mean: 

Hi, i'm doing a project and i need some information. It is possible to get an electrical diagram of the ST-LINK / V2 ?

MMark.1
Associate
 
2 REPLIES 2
LMI2
Lead

Many demo boards from ST contain something compatible. I have parts placement picture of STM32nucleo board (UM1724 page 12), which have it, and there are others.

ST doesn't sell ST-LINK/V2 STM32F103 parts, although binaries can be found to facilitate this.

The main difference between the on-board and external stand-alone devices is the use of logic level translation for the JTAG/SWD pins based on the VTarget provided by Pin 1 of the ARM 20-pin JTAG header.

I'm sure one could find a schematic for the boot-leg devices if you looked for them.

ST does offer the ST-LINK/V3 in a module form for placement on user boards. Perhaps review that.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..