2024-08-11 2:27 PM
What should I do when stm32 applications do not see st-link and the message I always receive is: Failed to start GDB server
Failed to start GDB server
Error in initializing ST-LINK device.
Reason: (2) ST-LINK DLL error.
No matter which stm32 board or cable I took result the same.
Solved! Go to Solution.
2024-08-11 6:02 PM
Perhaps a firewall issue.
Can STM32CubeProgrammer connect? OS? Software version?
2024-08-11 6:02 PM
Perhaps a firewall issue.
Can STM32CubeProgrammer connect? OS? Software version?
2024-08-12 11:20 AM
STM32CubeProgrammer does not connect. Windows10. Software - latest.
2024-08-12 1:08 PM
Okay, so not a GDB specific issue.
Can STM32CubeProgrammer see the programmer? Does it show a serial number, firmware version, voltage, etc? Does it show up in the device manager?
What board(s) are you trying? What programmer do you have? Are these custom boards?
2024-08-13 2:35 AM - edited 2024-08-13 2:38 AM
It seems it is firewall issue. I have to test it more. Thank you very much.
2024-08-14 2:27 AM - edited 2024-08-14 2:36 PM