Skip to main content
Associate II
May 28, 2025
Solved

Discontinuous SPI communication clock

  • May 28, 2025
  • 4 replies
  • 609 views

Using NUCLEO H723ZG

I made a simple SPI module for communication as master

(this is the only module i am using)

I used the MOOC training on using SPI as a guide for programming

On observing clock

I found it to be discontinuous during transmit cycle - this puts the receiving slave SPI into error

0x84 code

See Scope shots of clock

I was wondering if any one else has seen this before

Thanx in advance for any suggestions/replies

Jay

This topic has been closed for replies.
Best answer by JJAYAR

Hi TDK

The dma trick seems to have worked!

Thanx for your help

solved-will close this case now

Jay

4 replies

TDK
May 28, 2025

There is no issue in general with the SPI clock having delays between bytes. Most slaves have no issue with this. What chip are you communicating with?

If you don't want delays, reduce clock speed or consider using DMA.

"If you feel a post has answered your question, please click ""Accept as Solution""."
JJAYARAuthor
Associate II
May 29, 2025

Hi TDK

Thanx for replying

I was wondering

1) What would cause the clock to place delays ( i am not programmatically asking for delays)

The spi seems to be able to transfer about 13-14 words w/o delay

Why a new delay after 15th word?

2) Why would using DMA get rid of delay?

 

Also, The slave is a custom stm32H723 chip board

 

Jay

 

TDK
May 29, 2025

If the CPU can't keep up with data the SPI needs, there will be a delay between bytes.

Using DMA offloads this responsibility so no delays.

"If you feel a post has answered your question, please click ""Accept as Solution""."
JJAYARAuthorBest answer
Associate II
June 2, 2025

Hi TDK

The dma trick seems to have worked!

Thanx for your help

solved-will close this case now

Jay