Others: STM32 MCUs related

Find out more about STM32 implementations with external components, discuss use cases, and discover how to use new tools and ST components.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F411 and SD card read/write issues (SDIO)

Hi,I am running a code to expect to get a digital ouput (wave file from sd card) using amplifiermax98357a. when i run this code the only thing i got is a noise like burning wood. can i get any help. i am assuming the sd card not beeing read or initia...

mt19 by Associate II
  • 182 Views
  • 3 replies
  • 0 kudos

Resolved! Demo FYI: ESP32 AND STM32 I2C INTERFACE

 STM32 (I²C Master) → ESP32 (I²C Slave) “WASD” Command Link with UART InputSummaryThis project establishes a reliable data path from a PC to an STM32 microcontroller over UART, and from the STM32 to an ESP32 over I²C. The user types a line containing...

tantheman by Associate III
  • 524 Views
  • 6 replies
  • 2 kudos

I2C communication between STM32L4R5 and esp32

I tried creating I2C connection between my stm32 board and esp32. I assume it is not working because of my code, due to the wiring being so simple in I2C communication, the pull up resistor is connected externally. Do you guys see any mistake in my c...

ejeee by Associate
  • 3060 Views
  • 13 replies
  • 5 kudos

NRF24301 working library

Hello,Please suggest me some library for NR24L01 which is prefectly working. It should based on C language. I search few posts but many libraries are not working as I could see in comment section. Regards,Manoj Hiwarkar

Country of Origin Issues

Hello,We are facing COO issues with almost all STM32G4 and H5 MCUs. The website/invoice says COO is non china and when we actually get the products, the chip marking is CHN. When enquired, STMicro team bluntly emails saying CHN is not China. After 20...

Resolved! How to program an Olimex STM32-E407

I am having a hard time figuring out working with the STM32-E407 which is built on STM32F407ZGT6 MCU. I also brought an ARM-USB-TINY-H as it was recommended in its documentation. How and where do I start ? Say I want to interface this board with a ra...

mk_stm by Associate II
  • 420 Views
  • 10 replies
  • 5 kudos